AXIS#.SAFE.SBT.MOVE

Description

Executes Safe Brake Test (SBT) on the specified axis. All brakes attached to this axis are tested. A maximum of two brakes can be attached to a specific axis. For this command to work, Safe Brake Control (SBC) and SBT must be configured consistently in the SMM using safety parameters.

Code

--> AXIS1.SAFE.SBT.MOVE

Context

For complete information on SBT, refer to SBT (Safe Brake Test).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32
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
AXIS1.SAFE.SBT.MOVE

2fc0h

01h

Unsigned32

-

-

Write only

No

AXIS2.SAFE.SBT.MOVE

2fc0h

02h

Unsigned32

-

-

Write only

No